BRAKE#.STATE
Description
Reads whether the brake is released or applied.
Value | Description |
---|---|
0 | Brake applied |
1 | Brake released |
Examples
Context
For more information see Brake.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
---|---|---|---|---|---|---|
3105 |
1 |
3105 (0xc21) |
BRAKE1.STATE |
Unsigned8 |
Read Only |
Yes |
3106 |
1 |
3106 (0xc22) |
BRAKE2.STATE |
Unsigned8 |
Read Only |
Yes |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
BRAKE1.STATE |
3105 |
Unsigned8 |
Read Only |
- |
BRAKE2.STATE |
3106 |
Unsigned8 |
Read Only |
- |